The correct cutting speed for steel machining

The cutting speed describes the speed at which the cutting edge of the tool moves relative to the surface of the workpiece. It is expressed in metres per minute (m/min) and is one of the most important parameters in machining. Making the right choice has a significant impact on machining time, surface quality, tool wear and, consequently, the cost-effectiveness of the entire process. Which cutting speed is optimal depends on many factors. These include, in particular, the material to be machined, the tool material used, the machining process and the cooling system.

Why is cutting speed important in machining?

  • Tool wear and service life
    Choosing the right speed reduces the load on the tool, increases its service life and so lowers the cost of tools. A cutting speed that is too high leads to increased wear and can even cause the tool to break.
  • Heat generation
    A lot of heat is generated when working with steel. If the speed is set too high, the tool may overheat and lose its hardness.
  • Surface quality
    The correct setting ensures clean cutting areas. Values that are too low or too high can lead to chatter marks, built-up edges or a poor surface finish.
  • Process reliability
    Particularly with hardened and tempered steels, the correct setting is crucial for achieving consistent and reproducible results.

Calculating cutting speed

The cutting speed is calculated from the diameter and rotational speed using this formula:

Example:

Diameter: 12 mm
Speed: 3,000 1/min

vc = (3.14 × 12 × 3,000) / 1,000
vc = 113.04 m/min

Key:
vc = cutting speed [m/min]
π = pi (the mathematical constant)
d = tool diameter [mm]
n = rotational speed [1/min]

The difference between cutting speed and feed rate

Cutting speed and feed rate are two key parameters in machining which describe different movements. Whilst the cutting speed refers to the cutting edge of the tool, the feed rate (f) describes the speed at which the tool penetrates the workpiece or advances along the machining direction. It determines how much material is removed per unit of time and has a significant influence on chip formation, surface quality and the cutting forces involved.

Help with the calculation: The Meusburger cutting data calculator

Finding the correct cutting values is easy

1

Step 1: Select tool

From our wide range of cutting tools, select the tool you wish to use for machining your material, depending on the machining method (milling, drilling, thread cutting, reaming). Also select the appropriate tool diameter.

2

Step 2: Select machining method

In the next step, specify how the workpiece is to be machined (e.g. milling). In addition, please specify here the material to be machined, including the exact material number.

3

The result

Once all the data has been entered, the cutting data calculator automatically displays the values for tool diameter, cutting speed and feed. You will also be given a reference value for the rotational speed. You can then simply email the values to yourself.

1

Step 1: Select tool

From our wide range of cutting tools, select the tool you wish to use for machining your material, depending on the machining method (milling, drilling, thread cutting, reaming). Also select the appropriate tool diameter.

2

Step 2: Select machining method

In the next step, specify how the workpiece is to be machined (e.g. milling). In addition, please specify here the material to be machined, including the exact material number.

3

The result

Once all the data has been entered, the cutting data calculator automatically displays the values for tool diameter, cutting speed and feed. You will also be given a reference value for the rotational speed. You can then simply email the values to yourself.

1

Step 1: Select tool

From our wide range of cutting tools, select the tool you wish to use for machining your material, depending on the machining method (milling, drilling, thread cutting, reaming). Also select the appropriate tool diameter.

2

Step 2: Select machining method

In the next step, specify how the workpiece is to be machined (e.g. milling). In addition, please specify here the material to be machined, including the exact material number.

3

The result

Once all the data has been entered, the cutting data calculator automatically displays the values for tool diameter, cutting speed and feed. You will also be given a reference value for the rotational speed. You can then simply email the values to yourself.

Factors affecting cutting speed

The material

The material has a significant influence on the choice of cutting speed. Hard and dense materials, such as carbide, generate higher cutting forces and cause greater tool wear, which is why lower cutting speeds are required. Soft materials with good machinability on the other hand allow for higher cutting speeds and more cost-effective machining. Chip formation also affects process safety and heat generation.

The general rule is: the higher the hardness of the material, the lower the cutting speed should be.

The machining method

The machining method affects the load on the tool and therefore the choice of cutting speed. When milling, a higher rotational speed is usually possible. When drilling, deep hole drilling or for thread cutting and thread forming, due to the higher thermal and tool loads lower values must be selected. Reaming is carried out at medium to low cutting speeds in order to achieve high precision.

The cooling

Cooling reduces heat and friction during machining, thereby extending the service life of the tool. The inner coolant supply is particularly effective, as it cools the cutting edge directly. Minimum quantity lubrication can also effectively reduce friction. In general, adequate cooling enables higher cutting speeds and a more stable machining process.

The tool

Another key factor in choosing the cutting speed is the tool material. It determines which speeds are technically feasible and how well the tool can withstand the resulting loads. HSS tools (high-speed steel) are relatively sensitive to heat and are therefore only suitable for lower cutting speeds. Carbide tools, on the other hand, offer high wear resistance and heat resistance, which means that significantly higher cutting speeds can be achieved. Adjusting the tool material to the cutting speed is therefore crucial for cost-effective and reliable machining.

Discover our range of products for every machining method

Whether it’s milling, drilling, thread cutting or reaming: Our cutting tools are state-of-the-art and specially optimised for the requirements in mould and die making. 

Our product selection for you

WZF 28996 Karbür 3D full-radyus grafit için freze, gerilimi alınmış Ürün tek görseli
WZF 28996
  • Sonbahara özel teklif
  • Karbür 3D full-radyus grafit için freze, gerilimi alınmış
    WZF 12248 Karbür kaba/finiş parmak freze, uzun Ürün tek görseli
    Karbür kaba/finiş parmak freze, uzun
    WZG 171518 Metrik dişler için karbür klavuz, sert malzeme için Ürün tek görseli
    WZG 171518
  • Sonbahara özel teklif
  • Metrik dişler için karbür klavuz, sert malzeme için
    WZR 102520 Solid carbide high-performance reamer for through holes H7 Ürün tek görseli
    Solid carbide high-performance reamer for through holes H7
    WZG 32120 Kör ve patlayan delikler için HSS-E metrik makine klavuz Ürün tek görseli
    Kör ve patlayan delikler için HSS-E metrik makine klavuz

    Further exciting topics
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
    Yapılandırmak istediğiniz öğe bir 'e aittir. Ayarlamalarınızı yaptıktan sonra, tüm plakaları ve bileşenleri teknik uyumluluk açısından ayrı ayrı kontrol edin.