Long-term cost reductions through the use of a hot runner system

Hot runner or cold runner? This is a frequent question to which we are pleased to help you find an answer. You will see that a hot runner system will be the better choice in the long run.

Resources, plastic granulate included, become ever more valuable. With the use of a cold runner system there are inevitably high costs due to the unusable sprue. It is precisely these costs that must be avoided for more efficient production. Using a hot runner system saves on the cost of the unusable material. You can use our sprue cost calculator to calculate how much material costs could be saved in the injection moulding process.

Angusskostenrechner

Other advantages of a hot runner system

Given the current scarcity of raw materials and the price increase in plastic granulate, economic efficiency is even more important. By using a hot runner system, decisive application advantages can be achieved that have a positive impact on productivity. Although hot runners are often associated with higher procurement costs, there are many other technical and financial aspects that make them preferable to cold runners.

Technical perspective

  • Shorter cycle times, as sprues usually have to cool down for longer
  • Reduced loss of pressure
  • Improved holding pressure effect
    Positive impact on shrinkage and warping
  • Injection from the inside possible
  • Potential to use stack moulds

Financial perspective

  • Sprue spiders do not have to be sorted
  • No storage of runners required
  • No regranulation required
  • Less space required for the same production volume

Further information

If the advantages of a hot runner system outweigh the disadvantages for you, contact us and send us an enquiry. Our sales team is at your service. Alternatively you can also test our configurator for standardised hot runner systems.

商店选择

购物车预览

CAD 预览

您的购物车为空。
净额共计
至购物车
配置器加载时间超出预期。
请检查您的网络连接,然后重试。

重要提示

您要配置的项目属于。调整后,请独立核查所有面板与组件的技术兼容性。