Contact

Vă stăm la dispoziție personal cu cea mai mare plăcere de luni până vineri între orele 8:00 și 17:00. Pe acest link ve-ți regăsi persoana de contact din regiunea dumneavoastră.

Centrala Wolfurt
+43 5574 6706-0

Persoana dvs. de contact

Coş de cumpărături {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Articol   Schimbare coș cumpărături

Observație

Poză Articol Buc Preț unitar Preț total Preț total incl. reducere
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben:[{attrPrefix: 'L_', searchPattern: '/...', replacePrefix: '/', replaceSuffix: ''}] }} {{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

     
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

     

Vă rugăm să vă logați pentru a vedea prețurile și pentru a continua comanda.

O-ring seals - in perfect shape, part 1

Publicat la: 30.06.2020

General information and selection

In this first part, we explain the different sealing types, installation options and materials of O-rings especially for mould making.

O-ring seals are C-parts which cost only a few cents apiece. However, if an O-ring seal does not seal properly, it may result in downtimes and lead to high costs. To prevent this, in addition to the selection of the correct material, the design, the production of the O-ring groove and the correct installation, removal and maintenance of the O-ring seals are all important factors.

Use of O-ring seals

O-ring seals are mainly used in mould making to seal cooling holes used at plate transition or for components such as fountains and deflection elements. But O-ring seals can also be found in other components such as hydraulic cylinders and oil ports.

Dynamic and static sealing

A basic distinction is made between dynamic and static sealing. A dynamic seal is when the seal is created between components that move towards each other. O-ring seals are the optimum technical solution for dynamic sealing only in exceptional cases. For static sealing there is no movement between the components.

Axial and radial installation

The following figures compare axial and radial installation

Axial installation

Radial installation

In mould making, mainly static sealing is used with mostly axial installation. An example of this is the transition of the cooling holes from the cavity plate to the inserts.

Example of a mould insert

O-ring seal materials in mould making

The O-ring seals used in mould making are made of the material fluororubber - shortened to FKM, or FKM plus. FKM is generally very resistant to a variety of mediums and chemicals.

The selection of O-ring seal material depends mainly on the operating temperature. The usual FKM materials are used at water temperatures up to 100°C. If these were operated at water temperatures above 100°C they would harden, lose their elasticity and thus the pretension for the sealing effect. That’s why the special high-temperature O-ring seals made of the material FKM plus were developed for water temperatures over 100°C.

La noutăți
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
Now the new ‘My account’ also gives you a direct insight into the next level of the Meusburger portal. Check out all the information and benefits of the portal here.

Get familiar with our new ‘My account’ section and benefit from numerous advantages.

Now the new ‘My account’ also gives you a direct insight into the next level of the Meusburger portal. Check out all the information and benefits of the portal here.

Keep selection
Beta
New version
Current version