Yhteydenotto

Palvelemme sinua henkilökohtaisesti maanantaista perjantaihin 8.00–17.00. Tästä linkistä löydät alueesi yhteyshenkilöt.

Keskus Wolfurt
+43 5574 6706-0

Yhteyshenkilösi

Ostoskori {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Tuote   Vaihda ostoskoria

Huomautus

Kuva Tuote Kpl Yksikköhinta Kokonaishinta Kokonaishinta sis. alennuksen
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben:[{attrPrefix: 'L_', searchPattern: '/...', replacePrefix: '/', replaceSuffix: ''}] }} {{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

     
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

     

Kirjaudu sisään nähdäksesi hinnat ja jatkaaksesi tilaamista.

Tool holders for mould and die making

The requirements for a tool holder for machining in mould and die making are usually very different from those in contract manufacturing. We have taken a closer look at these basic requirements and the importance of tool holders as a component of a machine tool.

Workshop equipment

Requirements for a tool holder

Concentricity

To ensure high dimensional accuracy, central rotation of the clamped tool to the axis of the tool holder is essential. This prevents contact breakage between the material and the tool, which would lead to repeated impact on the tool and would subsequently cause micro breaks on the cutting edge of the tool.

Balance quality

A finely balanced holder is crucial for the spindle to run smoothly. In combination with the right tool, this ensures better workpiece surfaces, maximum tool life and longer spindle service life.

Radial stiffness

During machining, the milling cutter absorbs forces that transfer to the tool holder. To absorb these forces, it is especially important that the holder has a high radial stiffness . If this criteria is met, large infeeds and high speeds can be realised.

Repeatability

Every time the tool is changed, there is a risk of deviating from the original set point value in the axial positioning of the tool holder. That is why it is all the more important to reproduce the predefined value again with every tool change. This is an essential factor in achieving high workpiece precision .

To sum it up the interface between the machine and the tool is partly responsible for reaching long service lives and achieving the full performance potential of cutting tools in modern machine tools. What’s more, milling results with high dimensional accuracy and best surface quality are only achieved by the optimum combination of tool, workpiece, tool clamping equipment and machine tool.

Other important criteria

Interfering contour

Deep cavities and complex contours – these are hurdles that are often difficult to overcome in the machining of cavities in mould halves. The interfering contour of the tool holder plays a major role here. A low interfering contour allows the use of shorter tools. The result:

  • Higher cutting values
  • Better surface qualities
  • Longer service life

Projection length

Another point in manufacturing deep cavities is the projection length.
This is usually titled with dimension ‘A’ and is responsible for the tool reaching all the way down into the cavity. Thanks to our standard range of tool holders and the possibility of other projection lengths on request, Meusburger is the right choice.

Stability and damping

If high surface qualities are required during finish milling, stability and the damping properties of the tool holder play a major role. If the construction is not designed for the application or if a low-quality material is used for the manufacturing of the tool holder there will be significant effects on the results achieved.

Great savings potential due to the reduction of the eroding processes:

  • The surface is milled to gloss by hard milling so that only partial areas nearby still need to be eroded.
  • No subsequent eroding and polishing is necessary.

Maximum process reliability

The price for a finished mould half including cavity can quickly become expensive, and is significantly above the average market price of workpieces in conventional contract manufacturing, which makes it it even more important that no errors occur during production.

  • Process reliability requirements for high precision and qualitymust be strictly observed in mould and die making.



Here you can find the matching tool holders

You might find these topics and products interesting
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
Now the new ‘My account’ also gives you a direct insight into the next level of the Meusburger portal. Check out all the information and benefits of the portal here.

Get familiar with our new ‘My account’ section and benefit from numerous advantages.

Now the new ‘My account’ also gives you a direct insight into the next level of the Meusburger portal. Check out all the information and benefits of the portal here.

Keep selection
Beta
New version
Current version