Meusburger celebrates its anniversary at Fakuma

At this year’s Fakuma in Friedrichshafen from 15 to 19 October, Meusburger will focus on celebrating its 60-year anniversary. Moreover, the standard parts manufacturer will present its comprehensive range of plates, mould bases, components, and hot runner solutions as well as its newest products. Highlights at trade fair stand 2313 + 2316 in hall A2 will be the injection moulding machine with Meusburger standard parts live in action and the presentation of the new portal. Since it is also particularly important to the company to maintain existing partnerships and make new contacts, it will offer the possibility to visit Meusburger and get to know it better during a company tour.

Contacto para prensa

Julia Grimm Tel.: +43 5574 6706 1496 Dirección de correo electrónico: j.grimm@meusburger.com

Classics from 60 years

This year, Meusburger will take the opportunity at Fakuma to celebrate 60 years of standardisation with its customers. Classic products from the last 60 years will be the focus of the celebration. These include:

  • Mould bases for reliable solutions. Mould bases from Meusburger ensure the highest precision, thanks to the company’s constant optimisation process and decades-long experience.
  • Guiding systems for durable injection moulds. The company manufactures its guiding systems itself to ensure the best possible quality.
  • Slide units for numerous applications. The standard parts manufacturer offers a great variety of slide units, from the smallest compact slide on the market to slide units with temperature regulation and big slide construction kits.
  • Locks for time-saving work. Customers benefit from maximum flexibility with the ready-to-use locks.
  • Hot runner systems for demanding projects. Meusburger is the key partner for standardised hot runner solutions and customised complete solutions for complex projects.

 

Comprehensive range

The comprehensive range of plates and mould bases from Meusburger opens countless possibilities to its customers. Even the very best raw material is heat-treated for stress relief by the standard parts manufacturer, which ensures maximum quality for customers. Thanks to its high degree of in-house production and its vast warehouse capacities, Meusburger can guarantee its customers very short lead times. Moreover, the Austrian company’s customers benefit from high-precision components matching their requirements. The range not only includes guiding elements, but also numerous ejectors, slide systems, locks, and hot runner solutions. All in all, the customers can choose from more than 24,000 components. The product range is constantly being expanded, and the company’s team is always happy to advise customers.

Welcome to the next level

Apart from the ENGEL injection moulding machine, a highlight at this year’s trade fair stand will be the presentation of the Meusburger portal. The standard parts manufacturer has taken its online world to a new level so that its customers can reach their goal as quickly and intuitively as possible. With just a few clicks, the portal is easy to use for any target group and available 24/7. Customers benefit from time-savings in design thanks to wizards and configurators, a clear navigation, simple order processing and access to all order data and receipts. And that’s not it: Meusburger is constantly developing its portal and even more functions will be available in the future. Thus, the company is setting new standards for working with standard parts in mould and die making. Insight into the Meusburger portal can be gained here.

Company tour at Meusburger

During Fakuma, Meusburger invites all interested parties to a company tour in Wolfurt. An in-depth tour not only introduces visitors to the company, but also takes them through the production facilities and warehouses, thereby granting them an exclusive glimpse into the production processes and presenting the vast range of the leading manufacturer of high-precision standard parts. Moreover, Meusburger inaugurated its showroom in Hohenems in March this year: the interactive information portal, which can be explored individually by customers and employees alike, showcases the product range and the advantages of the company.

Vista previa del carrito

Vista previa CAD

Su carrito de la compra está vacío.
Total
Ir al carrito

Importante:

El artículo que desea configurar forma parte de un . Después de configurarlo, asegúrese de comprobar que todas las placas y componentes son compatibles desde el punto de vista técnico.