Try out the innovations directly
Mould makers can see the many innovations directly for themselves at the Meusburger trade fair stand. The E 8630 Gear unit for stack moulds can also be tested in installed form. This item convinces by the ground and induction hardened gear wheels and gear racks in module 3 and 4. In addition the newly developed E 2187 Isotemp® is exhibited at the trade fair. The high temperature hose ensures more safety during the injection moulding process through the new silicone sheath. In addition to these and other highlights, the GMT 6000 Precision cutting and grinding machine will be presented for the first time and put into operation live directly on site.
New standard bar length at Meusburger
Also new in the range are the standard bars in the lengths 300 and 1,200 mm. These are ready as of Fakuma for dispatch in the 18,000 m² finished goods warehouse. At Meusburger the bars and plates are heat treated for stress relief thus reduced plate warping during machining is guaranteed.
Tried and trusted Meusburger classics
In addition to the innovations, the tried and trusted products will again be presented at the Meusburger trade fair stand. The multifunctional H 1000 Clamping system has revolutionised the manufacturing processes in mould making and stands for high efficiency. The system enables precise clamping of the plates with repeatable accuracy in the µ range. The innovative H 4062 Assembly table facilitates repair and assembly work on moulds. By way of multiple air nozzles, an air cushion is created on the underside of the moveable plate supports. This enables light and easy movement of the tool halves. Both split line faces are freely accessible without having to reposition or turn them around, enabling efficient operating.
Further information on the product highlights
Uutisten yleiskatsaukseen