O-ring seals – in perfect shape

O-ring seals are C-parts which cost only a few cents apiece. However, if an O-ring seal does not seal properly, it may result in downtimes and lead to high costs. As well as the selection of the right material, important factors to help prevent this are the design, the production of the O-ring groove, and the correct installation, removal and maintenance of the O-ring seals.

 

General information and selection

Use of O-ring seals

O-ring seals are mainly used in mould making to seal cooling holes used at plate transition or for components such as fountains and deflection elements. But O-ring seals can also be found in other components such as hydraulic cylinders and oil ports.

Dynamic and static sealing

A basic distinction is made between dynamic and static sealing. A dynamic seal is when the seal is created between components that move towards each other. O-ring seals are the optimum technical solution for dynamic sealing only in exceptional cases. For static sealing there is no movement between the components.

Axial and radial installation

The following figures compare axial and radial installation

Axial installation

Radial installation

In mould making, mainly static sealing is used with mostly axial installation. An example of this is the transition of the cooling holes from the cavity plate to the inserts.

Example of a mould insert

Beispiel eines Formeinsatzes

O-ring seal materials in mould making

The O-ring seals used in mould making are made of the material fluororubber, shortened to FKM, or FKM plus. FKM is generally very resistant to a variety of mediums and chemicals.

The selection of O-ring seal material depends mainly on the operating temperature. The usual FKM materials are used at water temperatures up to 100 °C. If these were operated at water temperatures above 100 °C they would harden, lose their elasticity and thus the pretension for the sealing effect. That’s why the special high-temperature O-ring seals made of the material FKM plus were developed for water temperatures over 100 °C.

O-ring seal E 2130

  • Material: FKM (Viton)
  • Maximum temperature (water): 100 °C
  • Maximum temperature (oil): 180 °C

High temperature O-ring seal E 21311

  • Material: FKM plus
  • Maximum temperature (water): 180 °C (peak 200 °C)
  • Maximum temperature (oil): 180 °C (peak 200 °C)

 

Planning and designing

Axial installation – circular pocket or ring groove?

The circular pocket offers the easiest and most space-efficient way to introduce an O-ring seal. However, the disadvantage is that the O-ring seal is always in direct contact with the medium (e.g. water or oil). This reduces the service life and shortens the maintenance cycles.

O-Ring in Kreistasche - platzsparendO-Ring in Kreistasche - mehr Sicherheit
O-ring seal in a circular pocket: space-savingO-ring seal in a circular pocket: more security

Advantage:

  • Space-saving

Disadvantages:

  • Contact with medium
  • Abrasion
  • Dirt build-up

The ring groove, on the other hand, completely separates the O-ring seal from the medium and thus offers maximum service life and long maintenance cycles. For optimal introduction, we recommend using an O-ring countersink, but it may also be carried out using a milling cutter.

Advantages:

  • O-ring seal protected
  • Long service life
  • Concentric grooves when using countersink for O-ring

Disadvantages:

  • Requires more installation space
WZB 12112 Solid carbide countersink for O-ring seals
Solid carbide countersink for O-ring seals
WZB 32112 HSS countersink for O-rings Product single image
WZB 32112
  • Permanent deal
  • HSS countersink for O-rings

    Specifications for the groove dimensions

    The groove depth T1 is designed so that the cord size of the O-ring is pretensioned by 15-30%. The groove width B must guarantee that the cross section of the O-ring fills the groove to a maximum of 85% in order to provide reserves for swelling or thermal expansion. When pressure is applied from the inside, the O-ring seal should be in contact with the outside diameter, whereas when vacuum or pressure is applied from the outside, it should be in contact with the inner diameter.

    NutmaßeNutmaße

    Tip: O-ring seal with a tight fit in the plate

    The outside diameter D2 can be 1% to 3% smaller than the outside diameter of the O-ring seal, so that the seal is tightly fitted and will not fall out.

    In our groove recommendations, you will find the finished groove dimensions and the matching O-ring seals coordinated to the O-ring countersinks clearly displayed. This covers~ 90% of cases, saves time when searching and provides safety during use. For your own groove design, you will find the recommended dimensions T1 and B in the data sheet for the corresponding O-ring seal,  E2130 or E21311.

    E 21311 High temperature O-ring seal
    High temperature O-ring seal

    Radial installation

    For radial installation, we recommend a lead-in chamfer with 20°. You will find the appropriate dimensions T2 and B on the O-ring seal data sheet. When drilling crosswise to the installation hole, the edges must be rounded. The O-ring seal may be stretched up to 6% when installed. For installation, the O-ring seal can be stretched up to 20% for a short time.

    Beispiel eines Formeinsatzes

     

    Production of the O-ring groove

    Comparison: Production of the O-ring groove with a milling cutter or countersink for O-rings

    A direct comparison shows that considerable time is saved when the groove is introduced using a countersink for O-rings. Furthermore, the difference in quality is clearly seen in the following figure. When produced with a milling cutter, milling grooves are created which run at the bottom across the groove. This is not optimal for sealing. With our countersink for O-rings, on the other hand, concentric grooves are visible which make optimal sealing possible. This saves time and provides security.

    O-ring groove made with a milling cutter

    Milling grooves criss-crossing the groove bottom hinder optimal sealing.

    O-ring groove made with a countersink for O-rings

    Concentric grooves ensure optimal sealing.

    Countersink for O-rings at Meusburger

    The countersink for O-rings ensures good accessibility in pockets (e.g. inserts) right up to the edge. We offer two types of countersinks for O-rings:

    Grafische Darstellung eines O-Ring-Senkers in einer Tasche, z.B. einem Formeinsatz.

    Solid carbide countersink for O-ring seals WZB 12112

    • Best groove surface quality
    • Suitable for materials up to 54 HRC thanks to high-quality TiAlN coating
    • Dimensions coordinated to provide a perfect fit for the O-ring seal on the outer diameter
    • Available in the 4 most common sizes

    HSS countersink for O-ring seals WZB 32112

    • Can also be used on column drilling machines with the WZB 32113 pilot for countersink
    • Available in 10 sizes

    With our cutting data calculator you get the right cutting parameters in no time. To save you the time-consuming selection and matching of O-ring dimensions, O-ring grooves and matching countersink, you will find the appropriate combinations in our groove recommendations.

     

    Installation, removal and maintenance

    Installation and removal

    No sharp or pointed objects may be used during installation and removal. This would result in damage to the O-ring seal and the O-ring groove. In addition, make sure that the edges of the O-ring grooves are burr-free and rounded. We recommend the practical, 5-piece assembly tool set for O-ring seals V 28100. This not only saves you time, it also helps you with the installation and removal of O-rings in difficult and narrow installation spaces. A detailed description of how to use the tools can be found in our manual on the product page in the web shop.

    Maintenance

    In general, the O-rings should be replaced every time the mould is revised. When cleaning the mould, no cleaners with acetone should be used. This would cause the O-ring seals to become porous, which eventually leads to leakage in the mould. Our universal cleaner VCM 20 is optimal for cleaning O-ring seal installation spaces. Before inserting, check again that the O-ring seal will not be not fitted over sharp edges. Sharp edges should be rounded where necessary. When inserting, the O-ring seal can be stretched up to 20% for a short time.

    Person sprüht Reiniger VCM 20

    Storage

    When storing O-ring seals, the following conditions must be observed:
    The storage temperature should preferably be between +5 °C and +25 °C and at a maximum relative humidity of 70%. Direct sunlight or bright light should be avoided. UV-protected storage areas or closed boxes are ideal. According to ISO 2230, the shelf life of O-ring seals made of FKM is a maximum of 10 years.

    Shopping cart preview

    CAD preview

    Your shopping cart is empty.
    Total net
    To the shopping cart
    Loading the configurator is taking longer than expected
    Please check your internet connection and try again

    Important note

    The item you would like to configure belongs to a . After your adjustments, please check all plates and components independently for technical compatibility.