Material numbers for steel explained simply

In the world of mould and die making, the right selection of materials is decisive for the quality, service life and cost-effectiveness of a component. Clear identification is essential, particularly for material designations such as those used in the Meusburger range of steels. The material number – clear and unmistakable identification in accordance with European standards – helps to reliably classify steel grades and avoid misunderstandings. But how exactly is a material number structured, and what is the meaning of the individual digits?

In this article we provide a clear overview of how the material numbers are structured, how they are read, and why this system is particularly important in practical terms in connection with Meusburger steel materials.

Why are there material numbers for steel?

In an international context it is important that steel designations can be understood clearly and independently of the trade name. While for example ‘1.2312’ has the same meaning globally, the trade name may differ depending on the manufacturer.

The material number:

  • creates clarity,

  • facilitates comparability,

  • enables international classification,

  • prevents incorrect orders.

The first digit: The main material group

In mould and die making, the most commonly used material is steel, which is classified as material group ‘1’. This is why our list of materials is made up almost entirely of material numbers that start with a 1; only two aluminium materials start with a 3:

0 = crude iron
1 = steel
2 = non-ferrous heavy metals
3 = non-ferrous light metals
4–8 = non-metallic materials

Material selection made easy

We have the right material for almost every application in our range – from hot-work steel and steel for case hardening through to powder metallurgical grades and carbide. And if you would prefer a personal recommendation, our experts are always there and happy to advise you.

Optimum choice of materials for every application

Are you unsure which Meusburger material is the right one for your application? Our material selection wizard helps you to find the right material for your application quickly and easily. Thanks to intuitive operation and practical search filters you can find your way directly to the material that is optimally matched to your requirements.

Meusburger steel grades at a glance

As a standard parts manufacturer it is of central importance to us to make the right steel grade for almost every application available. Because selecting the right material is dependent on many factors such as load, environment and function.

Cold-work steels

Cold-work steels are used for moulds which generally don’t reach temperatures higher than 200 °C while in operation.

Cold-work steel from Meusburger

Hot-work steel

The continuous operating temperature of hot-work steel is over 200 °C, which is why hot-work steel offers the best properties for die casting moulds as well as moulds with which high performance plastics are worked.

Hot-work steel from Meusburger

Steel for quenching and tempering

Thanks to their carbon content between 0.20% and 0.65%, these steels are especially suited for quenching and tempering through heat treatment, which results in an optimum combination of strength and toughness.

Steel for quenching and tempering from Meusburger

High-speed steel

High-speed steel, or HSS for short, is a high-alloy tool steel with large amounts of alloying elements such as tungsten, molybdenum, chromium, and vanadium. They offer high resistance to adhesive and abrasive wear with high toughness as well as high resistance to pressure and high temperatures.

High-speed steel from Meusburger

Steel for case hardening

Due to the low carbon content of steels for case-hardening, they are ‘inserted’ into an atmosphere with high carbon content and heated. The result is a piece with high core toughness and surface hardness.

Steel for case hardening from Meusburger

Steel for through hardening

Steels for through hardening are delivered in a soft condition. They are good for further hardening processes, in order to change the mechanical properties of the steel.

Steel for through hardening from Meusburger

Free expertise

Our experts have worked intensively on this topic. Download the resulting white paper and discover their fascinating insights.

商店选择

购物车预览

CAD 预览

您的购物车为空。
净额共计
至购物车
配置器加载时间超出预期。
请检查您的网络连接,然后重试。

重要提示

您要配置的项目属于。调整后,请独立核查所有面板与组件的技术兼容性。