Meusburger: Plates & bars for the highest demands

Meusburger places the spotlight on its extensive range of plates and bars. The standard parts manufacturer presents a perfectly coordinated portfolio that meets the highest quality standards and offers impressively fast availability.

Kontakt na tiskové oddělení

Julia Grimm Tel.: +43 5574 6706 1496 E-mail: j.grimm@meusburger.com

Tiskové oddělení - ke stažení

Quality made in Austria

One of Meusburger’s key promises is the outstanding quality of its products. All plates are 100% manufactured in Austria. Highly automated production facilities and thoroughly trained personnel ensure manufacturing precision in the µ range. The basis for the high quality is the careful preparation of the materials. Right at the start, the sheet metal undergoes spectral analysis and a strength test. Subsequently, stress-relieving heat treatment in the in-house furnaces ensures low-deformation processing of the materials. This careful and reliable process is carried out to save customers time and money.

Meusburger sets standards in availability and material selection

Thanks to extensive storage facilities at headquarters and the largest central standard parts warehouse, Meusburger guarantees the continuous availability of its products. The majority of the plates and bars can be dispatched directly from stock, which means what customers order today is immediately dispatched. Meusburger also has an impressively diverse range, with plates in more than 30 different materials ranging from hot-work steel and steel for case hardening to powder metallurgical steel and carbide. In addition, the plates are available in various sizes and eight different standardised variations that are optimally aligned to customer requirements.

Standard or custom: Solutions for every requirement

Meusburger customers can choose between high-quality standard plates, which are immediately available and ready for use, and individually customised solutions. Customisation is made easy using the plate configurator offered by Meusburger. In just a few steps, customers can create their desired plate by precisely adjusting material, dimensions and tolerances, and whether square or round plates, even the most demanding projects can be realised. Features such as a check of entered values in the background, a material selection wizard, and interactive selection tables with illustrations provide help during the configuration. The eight standardised variations (variation 1 to 8) cover a wide range of defined machining options, from roughing or finishing to raw materials in custom dimensions. Thanks to optimised production processes, special plates are usually ready for shipping after three working days.

Comprehensive range complemented by bars and personal consultation

In addition to plates, Meusburger also offers universally usable bars in various dimensions and materials, which are available directly from stock. The material selection wizard helps customers choose the right material. Meusburger also offers personal consultation in order to find the optimal solution for every application.

Learn more at: www.meusburger.com/plates-bars
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
Chcete konfigurovat položku, která patří do . Po provedení úprav prosím samostatně zkontrolujte technickou kompatibilitu všech desek a komponentů.