Varukorg {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Artikel   Ändra varukorg

Anmärkning

Bild Artikel St Enhetspris Totalpris Totalt pris inklusive rabatt
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

{{(warenkorbItem.aktionsBruttopreis || warenkorbItem.bruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan {{(warenkorbItem.gesamtAktionsBruttopreis || warenkorbItem.gesamtBruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan {{(warenkorbItem.gesamtAktionsBruttopreis || warenkorbItem.gesamtRabattBruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

{{hannexItem.einzelpreis | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan {{::((hannexItem.einzelpreis * hannexItem.Menge) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction())}} Pris på förfrågan {{hannexItem.gesamtpreis | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan
Totalsumma exkl. moms.:  {{warenkorbCtrl.warenkorb.calcGesamtpreis() | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Pris på förfrågan

Registrera dig för att fortsätta beställningen.

More efficiency through standardisation

Application area, die making

Standard components have an enormous influence on the cost of a die set. Above all, standardisation offers numerous potential savings - but how exactly?

Successful standardisation begins in the design phase The world is becoming smaller – both logistically and economically. Globalisation increases the competitive pressure on die and mould makers, but also offers the chance to profit from orders in fast-growing markets. At the same time the innovation wheel is turning ever faster, which requires adaptability and flexibility from companies. The high cost and time pressure forces companies to constantly improve their efficiency. A high degree of standardisation along the entire process chain offers an excellent opportunity to drastically reduce costs and project lead times.

In the product life cycle of a die, it is important to take a holistic view of the costs. At the beginning of a project, possible savings should already be considered. The use of standard parts has a positive effect on the overall cost. Helpful questions are for example: are there die components which can be standardised? If so, what possibilities are there to fall back on for internally standardised parts or die set concepts? Could these be bought from an external standard parts manufacturer? There is a lot of savings potential here to gain clear competitive advantages.

The design phase is decisive

The costs of a die can be greatly influenced during the development phase, whereas towards the end of the process, in the series productions stage, it is almost impossible to reduce costs. The designer determines the machining sequence in the die. He or she decides how the individual machining stations or the feed are designed. In this phase, the production parameters with which the die will later work in the stamping workshop are set. In addition, the designer decides whether the die set is to be constructed from standard plates in stock or from order-specific special plates. The more standard parts used, the higher the percentage of fixed calculable costs.

Reach your goal quickly with digital wizards

The use of standard parts results in savings in all areas. This starts with the fast and reliable pre-calculation by means of the Meusburger die set wizards. With these tools, all necessary components for a project can be assembled quickly and easily and saved for later use. CAD data of complete die sets can be exported from the Meusburger web shop or offline shop to all common CAD systems with just a few clicks. This gives the designer more time to concentrate on the actual ‘critical points’ of a die.

Over 40,000 items to guarantee success

In the area of die making, Meusburger offers over 40,000 items, which are specially tailored to customer requirements. The low deformation material itself has a big influence on the manufacturing and maintenance costs of the die: thanks to the high-grade steel, which is heat-treated for stress relief, as well as exact form and position tolerances, subsequent costs can be reduced. Also the built-in components - such as active parts - perform important functions in the die. Buying these from external suppliers, rather than producing them in-house, offers significant additional savings and therefore long-term competitive advantages. The best time for putting this into practice is quite simply - now! 

TIPS & TRICKS FOR STANDARDISATION
  • Create quality standards through low deformation plates
  • Develop design guidelines
  • Reduce the variety of components used
  • Use standardised components and lower manufacturing costs
  • Create machining guidelines, such as predefined tolerances or dimensions 
  • Create standardised processes

 

Följande ämnen och produkter kan också intressera dig