Identifying industry requirements, developing new products and expanding and adapting the existing range: that is what keeps our product managers busy throughout the year. We place great importance on providing our customers with compatible standardised products and offering them options for individual adjustment. For this reason, last year we expanded our product range to a total of 93,000 items available from stock.
From our plates to our bars, all the way to individual categories in the area of 'components', our entire product range is always put to the test. How can we improve our range, what additional size is needed, how can we support the customer even better - these are just some of the questions that our specialists ask themselves.
For example, in 2018, there were a number of highlights for mould making, for example:
Another highlight is our new ejector configurator, which we launched in autumn. Intuitive operation and direct export of CAD data are just two of the advantages. We are very proud of this new configurator and are pleased that with it we have further simplified the process for our customers.
Ejector configurator
In die making we increased our focus on the 'modular concept' and 'transfer and large dies'. There are now two brochures based on this. Our goal was to combine and expand the range for different die concepts so that you can find the relevant products directly.
We have also put together the corresponding products online and created new areas so that the items are easy to find.
Tehnică modulară
Ștanțe mari și de tip transfer
Now even more bars: over 5,000 new sizes for standard, round, and square bars.
Detalii
La noutăți