Jesteśmy do Państwa dyspozycji od poniedziałku do piątku, od godz. 8:00 do 17:00. Pod tym linkiem znajdą Państwo osobę kontaktową obsługującą Państwa region.
Market innovations presented by Meusburger at the K trade fair
29.10.2019, Mould making
At this year's K trade fair in Düsseldorf, the Meusburger stand featured the new configurator for hot runner moulds. The new cavity pressure sensors and many other Meusburger products were also presented to visitors, alongside the unmissable hot runner and control systems, WBI Knowledge Management and ERP software.
At this year's K in Düsseldorf, the leading trade fair for the plastic industry, everything at the popular Meusburger stand revolved around the new configurator for hot runner moulds, which is available exclusively at Meusburger. The complete mould base including hot runner manifold can be customised with just a few clicks and shipped shortly thereafter in the usual high quality in just one order. In addition to the hot runner mould, the required components and matching accessories can be ordered directly from Meusburger. During the K, the many visitors to the Meusburger stand learned about the benefits of the new configurator.
New sensors for more process reliability
As their second product highlight, Meusburger presented their new cavity pressure sensors. The sensors are immediately available from stock, and represent a further step towards industry 4.0. They offer maximum flexibility through direct or indirect cavity pressure measurement and are compatible with all common piezoelectric pressure sensors. Another benefit: the small installation spaces ensure a high degree of freedom in the mould design.
Everything from a single source
The PSG branded product range for hot runner and control systems also offered a lot for visitors. While in the field of hot runners the focus is on customised solutions, in the field of control systems when it comes to reduced cycle times, rapid colour changes, and gating of difficult to reach parts the profiTEMP+ hot runner controller impresses with state-of-the-art technology and space saving design.
Digitalisation has arrived
As a digital addition to the range, WBI Knowledge Management presented their software specially developed for the Knowledge Management Method at the Meusburger stand. With the help of this software, the resource of knowledge can be collected, shared, further developed and saved. At the same time, the ERP software SEGONI.PPMS was presented to visitors, which is used for efficient production planning and focuses on companies with individual production structures active in the fields of mould, die, and jigs and fixtures construction. Thanks to these digital tools, Meusburger helps their customers to achieve sustainable success along the entire value chain.
Przetestuj naszą nową wersję zakładki "Moje konto"
Zapraszamy do zapoznania się z nowym obszarem „Moje konto” i skorzystania z jego licznych zalet.
Poprzez "Moje konto" możliwy jest także bezpośredni dostęp do kolejnego poziomu, nowego portalu firmy Meusburger. Wszystkie informacje na temat portalu i jego zalet można znaleźć tutaj.
Zapraszamy do zapoznania się z nowym obszarem „Moje konto” i skorzystania z jego licznych zalet.
Poprzez "Moje konto" możliwy jest także bezpośredni dostęp do kolejnego poziomu, nowego portalu firmy Meusburger. Wszystkie informacje na temat portalu i jego zalet można znaleźć tutaj.