Contact

We are available for you from Monday to Friday from 8:00 to 17:00. Use this link to find the contact persons for your region.

Your contacts

+43 5574 6706-0

Your message:

Shopping cart {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Items   Change shopping cart

Remark

Picture Items Pcs Single price Total price Total price incl. discount
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

{{(warenkorbItem.aktionsBruttopreis || warenkorbItem.bruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request {{(warenkorbItem.gesamtAktionsBruttopreis || warenkorbItem.gesamtBruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request {{(warenkorbItem.gesamtAktionsBruttopreis || warenkorbItem.gesamtRabattBruttopreis) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

{{hannexItem.einzelpreis | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request {{::((hannexItem.einzelpreis * hannexItem.Menge) | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction())}} Price by request {{hannexItem.gesamtpreis | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request
Total, VAT not included:  {{warenkorbCtrl.warenkorb.calcGesamtpreis() | currency:warenkorbCtrl.warenkorb.waehrung:warenkorbCtrl.warenkorb.getFraction()}} Price by request

Please log in to continue with the ordering process.

Lowering tension

In our selected range you can find the right material for virtually any application.

Franz Kohler
Head of Product Division

We heat treat properly for your success

Not all stress-relieving heat treatment is the same – because only a proper heat treatment process ensures the desired result in the end. That is why Meusburger has been using its own furnaces for almost 30 years.

Since the quality of the sheet metal is decisive for the subsequent machining of the plates and bars, Meusburger places the highest demands on their steel suppliers. And because twice is better than once, all sheet metal is subject to both a spectral analysis and a strength test directly on the premises to check the quality. Only flawless steel from the best-known steelworks can make it through the quality check at Meusburger and thus into one of the three in-house furnaces. These have a total capacity of 240 tonnes per day.

The strength lies in rest

Already during the production of sheet metal, tension builds up in the material for example during rolling and cooling of the sheets. In order to reduce this to a minimum, in addition to the controlled heating of the sheet metal and the maintaining of the temperature at approximately 580°C, it is especially the uniform cooling that is decisive. At Meusburger the entire heating process, which lasts about 24 hours, takes place in a closed furnace. The slow and continuous cooling of 35°C per hour ensures uniform cooling of core and surface zones and thus prevents the build-up of new tension while both the microstructure and the mechanical strength of the material remain unchanged.

Less deformation, HIGHER PRECISION

The procedure, from the precise inspection of the sheet metal through to the perfectly executed stress-relieving heat treatment, guarantees low-deformation processing of Meusburger products. The tension in the material is reduced to a minimum. This advantage is reflected in the end product and in the machining time. Dimensional and shape changes during subsequent heat treatment processes are reduced, whereby the allowance can also be reduced.

The resulting shorter machining time and longer service life allow for free capacity for other tasks. If the components are not subjected to any further heat treatment, the advantage of low-deformation processing is even greater because the plates retain their dimensionally stability even after a machining process. This makes it easier to keep the tolerances required and obtain high-precision components.

Stress-relieving heat treatment therefore reduces lead times, increases precision, results in cost savings and thus provides a competitive advantage in the long term.

Three furnaces for 240 tonnes of steel

Advantages of stress relieving heat treatment

  • Low-deformation processing
  • Shorter machining times due to reduced oversize
  • Longer service life of tools
  • Highest precision 
  • Advantages in automated processing, particularly when using clamping systems

Web shop