Meusburger Formaufbauten Wir bringen Stahl in Form
Sections
Produkte_Stichmass_H.jpg

The Meusburger coordinates

Meusburger sets benchmarks in European mould making
This systematic coordinated measure provides a continuous measuring system from the smallest through to the biggest standard mould. Big improvements are often achieved by simple and obvious ideas. Everything at Meusburger is done with the benefit for the customer in mind.

Cooling holes can be inserted between the guiding bore and the screw holes of any size of mould. The edge distance will remain the same for each guide diameter.The standardised coordinates of all Meusburger moulding plates as well as the sliding core moulds follow the same principle and offer many advantages to the customer.

The Meusburger coordinates (guiding bores and screw holes)




Customer Feedback

"For the system hole diameters, Meusburger offers a uniform distance from the plate edge.Nevertheless, the distance between system hole and tool fitting holes is such that there is enough space for the cooling hole. In my experience this is required in 90 percent of cases and thus is Meusburger's decisive advantage over other suppliers."
Frank Zachlod, design engineer at Pro Forma Leistungen für den Werkzeugbau GmbH in Radeburg (D)"

"The Meusburger coordinates are significantly more precise than others, which naturally has a positive effect on the quality of our moulds."
Otmar Gutmann, managing director of COLOR METAL GmbH in Heitersheim (D)

Artikelaktionen