Meusburger
Presseabteiltung Meusburger

Press releases

In this section you will find press releases regarding our company and new products, as well as your contact for press enquiries.

Are you interested in a specific topic? Choose from our news categories:

If you would like you to receive news from Meusburger regularly, subscribe to our Press distribution list.


E 1845 Round latch lock for space-saving installation in the pillar hole

E 1845 Round latch lock for space-saving installation in the pillar hole

The new E 1845 Round latch lock for installation in the pillar hole is now available from Meusburger. Its space-saving installation enables a high degree of flexibility when designing the cavity and the integration of temperature regulation components or slide units, and thus a more compact mould structure. Another advantage is the damping element on the stroke limiter of the round latch lock which enables especially fast plate movements. The tried and trusted system with four switching segments guarantees secure and reliable locking of the floating plate. With the E 1845 Round latch lock from Meusburger the stroke length is individually adjustable.


Gas springs with small to very high initial force

Gas springs with small to very high initial force

Meusburger is broadening its range of products for die making with a wide range of gas springs featuring small to very high initial force and matching accessories.

Gas springs are cylinders filled with nitrogen and use highly pressurised gas for providing the spring force required. The new product group consists of E 6350 Force, E 6320 Mini, E 6360 Force extreme and the spring plungers E 6310 and E 6315.


Centring vices for clamping without pre-stamping

Centring vices for clamping without pre-stamping

The expert in standard components has expanded his range of workshop equipment for die and mould making with the HWS 400 and HWS 402.

Through their particularly easy and reliable clamping these are suitable for first and second side machining. Due to the pull-down effect produced by the claws no pre-stamping of the workpiece is required. The low clamping heights of 3 to 5 mm for the stepped jaws and stepped jaws with claws ensure low material requirement.


Meusburger erweitert Materialqualitäten bei den NP – Präzisionsstäben

Meusburger erweitert Materialqualitäten bei den NP – Präzisionsstäben

Präzisionsstäbe sind grundsätzlich für vielseitige Anwendungen im Werkzeug-, Formen- und Maschinenbau geeignet.

Um auf Kundenwünsche zu reagieren hat Meusburger ab sofort zwei zusätzliche Materialqualitäten bei den NP – Präzisionsstäben in das Programm aufgenommen. Die Qualitäten 1.2767 und 1.2363 werden standardmäßig in der Breite parallel gefräst und in Stärke geschliffen und sind ab Lager lieferbar.


E 55301 Mounting sleeve for bottle-neck cutting punch

E 55301 Mounting sleeve for bottle-neck cutting punch

Meusburger adds the E 55301 Mounting sleeve from pre-toughened tool steel 1.2312 to its selection of punching tools. The new product is complimentary to the E 5530 Bottle-neck cutting punch, which was specially developed for high punching and retracting forces. The special shape of the punch head prevents compression and the breaking of the head. The E 55301 Mounting sleeve allows for an easier insertion of the bottle neck contour in the punch retainer plate. Only a cylinder recess is required for the installation of the cutting punch. As usual with Meusburger, the new product is available from stock.